Hi,
We're considering use of the TS3L110 for multiplexing four wire 10BASE-T ethernet connection to two devices. Can the TS3L110 be used to switch the copper carrying the Ethernet signals prior to the RJ45 connector, or must this device be placed after the magnetics? The desired application is show below:
Any advice on this device, or others which may be more suitable would be appreciated.
Thanks,
James.