Dear all
I have 4 analog signals (0-2 Vpp range) coming from 4 Ultrasonic transducers with a frequency of 5 MHz each . I would like to multiplex them and send through a single line (1 meter length) .
At the end I'll have to demultiplex the Mux channels into the original 4 signals . Going to the TI selection of
MUX/DEMUX I can't find the right combination of 2 . Is that anything somebody already faced ? Any advise ?
And what if I would like to Mux and Demux 8 analog signals (same frequency BW) instead of 4 ?
I mean Time division mux but other alternatives could be acceptable.
Thanks to all
Max