Looking to confirm if the TS3DDR3642 currently in "Preview" status is available to support immediate engineering work to prototype a design followed by a ramp to modest volumes by the summer of 2014. If so, is it possible to get the full data sheet. Only a product preview is posted to the www as of Feb 21/14. Release to production time frame would also be helpful.
Also looking to confirm if the TS3DDR3642 will be pin compatible with the TS3DDR3812. I understand both parts are in the same package but the pin out of the TS3DDR3642 is not provided in the posted documentation.
Many thanks.