Hi,
I have a circuit design with 16 electrodes. One electrode pair is used for current excitation (10mA) while the remaining are used for potential measurements (PM). The frequency varies from 1kH to 500kHz. However for PM it requires reference potential which is adjacent of the excitation pair. The maximum potential difference between electrodes is 2.5V.
My problem is multiplexing the reference potential as the value occurs at all terminals nIN- (n=1,2,3...16) simultaneously. I come up with the schematic and would like to know if the output from MPC506AU which I connected is correct. For simplicity I only show the first 2 out of 16 connections which are (1IN- and 2IN-). Any suggestion or advice is much appreciated.
Regards
Fazlul