Looking for a +/-12V SPDT Analog Switch, preferably one that can be powered by a single supply instead of +/- split rails. What do you recommend?
By the way, the function of this device is to detect and switch a pair of inputs after detecting whether or not it’s an RS485 +/-12V signal or a +5V/0V digital line.
If a +/-12V signal input is detected, it’s routed through a level shifter to bring the voltage down and feed it into the MCU's interface input for processing. If the input is determined to be a 5V/0V digital signal, it’s thrown to the other output and routed directly to the MCU’s GPIOs.
Therefore, as a side note, please let me know if you’ve heard of any integrated solutions that could provide this functionality.
Thanks,
Jason