I have a need to switch between an LVDS (differential voltage of 600 mv with common mode of 600 mv) signal and a CMOS signal level of 3.3 V. The switching signal ideally is 2.5 V but I can make it what ever it needs to be.
I found the TS3DS26227 and it appears to be exactly the type of part I am searching for but I'm a little nervous that it would have an adverse effect on the LVDS signal. So was looking to understand if there is something specifically designed for handling LVDS signals.
Thank you,