This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I need a signal switch with more than 6 channels

Other Parts Discussed in Thread: TS3A27518E-Q1, SN74CBT3383, TS3DDR3812, SN74CBT3383C, SN74CBTLV16800, TS3DV642, SN74CBTS16212

E2E,

I am in need of some analog switches to mux pins for additional peripherals; the TS3A27518E-Q1 looks interesting.  Signals are likely just 1.8-3.3V levels, and the 1:2 switch function is needed – looks like this is a 6ch part, do you have any wider parts to recommend or is 6CH the most.  A-grade desired. Signals likely single-ended and sub 100MHz.

Thank you,

Adam