This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3T3253 higher current opperation

Hi,


I'm testing a sample of SN74CB3T3253PWR a dual 1:4 FET MUX/DEMUX. I was able to get the mux working for 1A; however, for 2A it only worked when I put both S0 and S1 on HIGH. What can be the cause of this? I am using 3.3V for Vcc and for logic. Thank you