This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Page 4 of the datasheet states: (1) All unused inputs of the device must be held at VCC or GND to ensure proper device operation. Refer to the TI application report, Implications of Slow or Floating CMOS Inputs, literature number SCBA004.
and then in the test section, page 10 states: All unused analog I/O ports are left open.
and page 11 states: All unused analog input (A) ports are left open, and output (B) ports are connected to GND through 50-Ω pulldown resistors.
These statements are conflicting. Should the unused pins be left open, or connected/terminated?
~Leonard
I've always considered DVI (DIGITAL Video) the same as a logic signal, it is not analog. It does seem that the overall performance of the device is affected by the unused 'A' signals being terminated, as it shows up in the cross-talk test, yet in the and ISOLATION and BW tests, 'A' is open. I think some clarity is needed in this regard!
~Leonard