I am using the IC (TS5A23159 - http://www.ti.com/product/TS5A23159) for the demultipelxing application in my circuit. The exact values of the input and output impedance of the demux is not mentioned in the datasheet. It is common that the ICs today have high input impedance and low output impedance for complete transfer of the signals. But the circuit I am using is very sensitive and I need to have the details of input and output impedances of each and every component that we have used in the circuit. So I request the experts in this forum to help me out with the details of input and output impedance of the IC (TS5A23159)