This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A3159 Analog Switch Issue

Other Parts Discussed in Thread: TS5A3159

Hi,

I am attempting to design the TS5A3159 into a product, as a replacement for two mechanical switches. I am having some problems and I think it is related to the the switch common (pin 4) going 0.5V below our digital ground, which is used as a ground for the device (pin 2). Our product is a loop powered (4-20 mA) and so there is ground and there is ground... Have you seen this issue and do you have any suggestions about a workaround?

Thank you

Rich