This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Crosstalk of TS3A226

Other Parts Discussed in Thread: TS3A226AE

Hi Team,

Since no matter which grounding FET is on, the both channels of LR headphone are sharing the same FET. So the rdson of the FET will make the crosstalk worse. So Lenovo want to know the crosstalk performance with 16ohms and 32ohms loads. Will you help?

  • Hello Peter,

    Thank you for your question.

    So Lenovo want to know the crosstalk performance with 16ohms and 32ohms loads. Will you help?

    Absolutely.

    Calculating Crosstalk: 20 * LOG(Vgnd/Voutput)

    Voutput = 1 Vrms

    Vgnd = Voutput * ((Rtrace + Rjack + Rgndfet)/ ((Rtrace + Rjack + Rgndfet) + Raudio))

    Assume 25 mOhms for both trace and jack contact resistance.

    16 ohm crosstalk without TS3A226AE : -50.13 dB

    16 ohm crosstalk with TS3A226AE : -43.31 dB

    32 ohm crosstalk without TS3A226AE : -56.14 dB

    32 ohm crosstalk with TS3A226AE : -49.31 dB

    Regards,

    Jared