This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A226AE recommended footprint



Hi Team there is not any design files on the CAD page for this part, can I get some information as the customer is starting their layout of this device.

Thanks in advance

  • Alan,

    Please use the following information for the 3x3 0.4mm pitch array:

    PCB: 0.23mm dia pads with 0.05mm max solder mask ring (for NSMD pads).
    Stencil: 0.25mm square paste openings with 0.05mm radius rounded corners
    0.1mm (0.004") thick stencil

    Thank you,
    Adam