I am trying to multiplex 4 sensors using UART communication to an Arduino Serial input. I only need to communicate with one serial device at a time and need to be able to select which device to communicate with. The devices are operating at a buad rate of 9600.
I was suggested to use a CD74HC4052 HIgh-Speed CMOS Differential Multiplexer/Demultiplexer. Would this chip meet my needs or should I use another one?