This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DV642 - Maximum skew

Guru 19785 points

Hello Team,

I can find TYP inter/intra-pair skew data in the datasheet, however, do you have maximum value for these skew ?

If no characterization data, it would be a great help if we could have the estimated or simulated maximum data.

Thanks in advance.

Best Regards,

Kawai

  • Takushi,

    I found some data where we tested these channels on three different ICs at 25 deg C with Vcc = 3.3 V. Of the 42 data points, the max value in this data set was 13ps, the min value was 0.1 ps, and the average was 3ps.  You can use this information for your reference but this post does not guarantee these values.

    Thank you,
    Adam

  • Hi Adam-san,

    Thank you for the information. Yes, I understand that those value are not guaranteed, just for information.

    Best Regards,
    Takushi