Hi Team,
When the TS3USB3000 switches from one channel to the other, I would like to understand the behavior of the path that is no longer connected to the output. My main concern is signal reflection..
Lets say that I am driving a signal into the USB +/- pins with the output at the D+/- pins, then I flip my switch so that I am driving a signal into the MHL+/- pins with the output at the D+/- pins. The signal that is being driven into the USB+/- pins is still being driven into the pins but is no longer connected to the output (D+/- pins), thus I am not sure what will happen to the signal at that point.. Is there some sort of internal termination, or will I get signal reflection?
For instance, the DS10CP152Q is a switch that contains output termination to minimize insertion and return losses, does the TS3USB3000 have something similar?
Thank you,
Jared