This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you recommend analog MUX with 1.8V operation?
12 inputs go into 1 output. one chip solution is ideal. Discrete solution is acceptable.
Yoshiki-san,
I found a couple 1:16 muxes on the TI.com switch selection tool like the CD4067B that will pass 1.8 V signals through the signal path.
What type of signal are you trying to pass through the 1:12 mux?
Do you have any other performance requirements of the switch other than passing 1.8V signal? Bandwidth, datarate, on-state resistance, etc?
Thank you,
Adam
Aozer,
Currently we do not have a 1:12 mux that will operate with a 1.8 V supply. Are you able to use a different voltage rail or a boost converter?
When I filtered the TI.com switch selection tool it returned 60 other muxes that operate with 1.8V supply. Like your current solution you could get creative using multiple ICs.
What do you think about using 3x TS3A44159 devices or 2x TS3A127518E devices to create a 1:12 mux?
Thank you,
Adam