This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kill Switch with Relay

Hello,

I'm looking to create a kill switch using a relay. I have a switch but it only supports around 5 amps. This project I'm working on have circuits that draws more than 20 amps. I want to have a kill switch for emergency. I was thinking on using the toggle switch to signal a relay of high amp that will open the circuit so no current is drawn. I don't know how relays work, maybe someone here could help on the diagram of this idea if possible. 

Thanks in advance. 

  • Emmanuel,

    Wikipedia says, "A relay is an electrically operated switch. Many relays use an electromagnet to mechanically operate a switch, but other operating principles are also used, such as solid-state relays. Relays are used where it is necessary to control a circuit by a separate low-power signal.

    The simplest relay I can think of is a piece of metal in a mechanical switch that can be moved by a magnetic field to open or close a circuit.  You can use a low power signal to energize an electromagnet that will control the piece of metal that can handle much larger currents. 

     For your application question on how to control a relay will be entirely dependent on the type of relay you choose.   I bet you could find a relay that could be controlled by a 3.3V signal that you could control with a toggle switch.

    Thank you,

    Adam