A server is muxed to a port of two GBE Switches through a TS3L501E.
When the path of the TS3L501E changes, the new connection to the Ethernet switch sometimes puts the Switch in a state where it wont pass any data.
The failures rates is about 1 in 10 SEL toggles.
If the path is not changed after power up, the two Ethernet switches operate normally.
Could some on-going data transfer at the moment of the path change be affecting the Switch that gets connected?
Is there minimum disconnect period, or PD mode period, recommended before connecting the server to a different switch?
Thank you