Hi,
We want to introduce SN74CB3Q3245PWR in place of IDTQS3VH245 for CPCI based Hot Swap Application in several of our boards.
Will it be possible to use it in direct replacement?
Please inform urgently.
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We want to introduce SN74CB3Q3245PWR in place of IDTQS3VH245 for CPCI based Hot Swap Application in several of our boards.
Will it be possible to use it in direct replacement?
Please inform urgently.
Regards.
Arm,
I typed in IDTQS3VH245 into the ti.com cross reference tool and it returned SN74CB3Q3245 as a direct replacement.
Thank you,
Adam
ARM,
There is a specification in the datasheet that states there is good isolation on the signal path with Vcc =0V. The term hot swap isn't very specific to me and can be vague but having isolation on the signal path without power to the IC tells me there is no power sequencing issues and you may add or remove this device from a powered up system without issue.
Thank you,
Adam