This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A26542: operation at Vio=+5V.

Part Number: TS5A26542


Hello

can the switch I\O operate at Vio=+5V , IN1,IN2 = Vio levels (0 & +5 V)

consider the max Vio should be less than 6.5V ,it shouldn't be a problem .

i would like to validate that

thanks

Gil Rafalovich