Hi,
I am planning to use the TS3DV642 switch in the following configuration.
Switch Input - 1x Input
Switch Output - 2x Outputs
Input is connected to a host in which HDMI 1.4/DisplayPort 1.2a signals are muxed. At a time, I can configure the controller for HDMI or DP output. The 2x outputs from the switch are connected to HDMI connector and Displayport connector and it will be controlled by GPIOs.
The signal mapping of HDMI/DP Data pairs in connectors is not exactly same, however if connections from switch output to the corresponding Display side connectors are taken care, then is this design is feasible? please confirm.
Regards,
Shareef