Part Number: SN74LVC1G3157
We've found a case where we're using the sn74lvc1g3157 outside of the specification and were hoping you could point us at some clarification.
The datasheet calls out a Vin maximum on the IO pins as Vcc +0.5V with a footnote saying "The input and output negative-voltage ratings may be exceeded if the input and output clamp-current ratings are observed." This specific application is @ VCC 2.5V, ideal use case is 0-3.3V.
Can you help confirm/help detail out potential impact, if any at all.