This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

beat Vishay DG201BDY-T with a +/- 12V switch

We found out a SPST analog switch opportunity for Inkjet Printer . Currently customer is using Vishay DG201BDY-T (4ch SPST) x2units for their 8ch SPST requirement in first prototype. We would like to beat Vishay with your analog switch, so could you check below requirements and let us know the best proposal?

 

< Requirements for Analog Switch >

  • 8ch SPST (two 4ch SPST is OK)

  • +/-12V supply voltage rating

  • Ron=<50ohm

  • Ranita,

    The current TI portfolio have very limited device selection at the +/- 12 V supply range. The only devices that operate at this range are the MUXXXXXX, MPCXXXX, or CD4XXX family of switches. In these families however there isn't a 1:1 device they are mostly 4:1 or 8:1 devices. We will log your request into our creative back log to release products with this configuration in the future.

    Thank you,
    Adam