This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5V330C: The AC coupling capacitor on output(Dx)

Part Number: TS5V330C
Other Parts Discussed in Thread: TS5V330

Hello,

 

Regarding to the AC coupling capacitor on TS5V330C, my customer is asking a question.

(Question)

・They will use it on output (Dx) of TS5V330C.

Is it supported ? and is there any problem with large value capacitor (ex.470 or 1000uF)?

 

Regards,

Tao2199

  • Tao,

    The TS5V330 is a passive FET switch and may be properly operated with or without external components as long as the datasheet specifications are satisfied.  You may put a AC coupling capacitor on the signal path without issue as long as there is a DC bias somewhere on the other side of the switch keeping the signal above 0V.

    Why do you need to have a large AC coupling cap with this switch in your system?

    Thank you,

    Adam