This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS12A4516: Theta JC (Junction to Case)

Guru 29720 points
Part Number: TS12A4516

Hi Team,

Could you tell me the value of Theta JC (Junction to Case) for TS12A4516DBVR?
I would also like to ask Tj-max for these.

Best Regards,
Yaita

  • Hello K. Yaita,

    Thank you for considering to use Texas Instruments in your design. We currently do not have that information on file for this particular device. However, we will perform the necessary test to obtain that information. It may take up to week for this product to go through the queue for this particular test.

    May I ask what you plan to use this device for or at least what are the requirements you want for your switch? If we cannot provide you with the necessary junction to case and Tj-max information soon enough, perhaps I can provide you with an alternative.
  • Yaita,

    You may also want to check out this link on how to calculate the max junction temperature for a signal switch.

    Thank you,

    Adam

  • Hi Adam-san,

    > If we cannot provide you with the necessary junction to case and Tj-max information soon enough, perhaps I can provide you with an alternative.
    I believe Theta JC (Junction to Case) is dependent on the package (SOT23-5).
    Could you tell Theta JC of another SOT23-5 device as a reference?

    My customer wants to know Theta JC only as a reference, so it doesn't need to be strict value in this case.

    Best Regards,
    Yaita / Japan disty

  • Hello K.Yaita,

    Below are the thermal characteristics of the TS12A4516: