Hi,
In the datasheet of SN74CBT162292, it is mentioned that the part has internal pull down resistors. Iam connecting one voltage divider to this mux .
pull up voltage = 3.3V
Rpull up = 806 ohm
Rpull down = 10K ohm
I need an output voltage of 3V. In this calculation I didn't consider internal pull down of 500 ohm. Shall I consider this also into the calculation , to get correct voltage divider voltage?
Regards,
Bhavya