Other Parts Discussed in Thread: TS5A3166
Hello.
There are two question about TS5A3166-Q1
1. Signal Transition
I did the experiment of clock signal transition.
I inputed clock signal at "COM" port [VIH 0.5V, VIL 0V, Frequency 20MHz, tR/tF 100ps (20%-80%)]
I measure it at "NO" port.
a. On state: OK
b. Off state: I expected that no signal was measured, but there was signal transition during about 3ns (max level 0.3V).
Question) Is this proper operation of this IC? I think that this is related to off isolation spec. Am i right?
And what is the input signal condition not to transit any(or very low level) signal?
2. IBIS Model
I got the IBIS Model on TI site and I opened it with Mentor company IBIS Model Editer (Viewer)
I tried to check the switch On/Off characterics. But I couldn't opened "[Model]TS5A3166_B_18_S]"
Please let me know how to see it.
And confirm that this IBIS file is not operated on Power SI toool.
Thanks.