I need switching IC to reverse the polarity of DC latching solenoid of maximum operating voltage is 24 and max operating current is 1A. IC should have low quescent current and it should operate on 4.2 volt battery.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hunter DC latching solenoid (p/n 458200) and it can be operate on 3.7 volt minimum when using the 4.2V battery.
Hi Sagar,
I am assuming you have settled on devices that operate from 3.7 to 4.2V.
Please take a look at the DRV8834. This device can drive two latched solenoids.
For a single solenoid, the DRV8847 DRV8837 would be a good choice. (Corrected part number -- 27 May)
We do not offer a device that can operate from 3.7 to 24V. The DRV8848 comes close (4V to 18V, with the ability to drive two solenoids).