This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Part Suggestion for a 16:1 Analog Multiplexer for 60mA of switching Current

Other Parts Discussed in Thread: TS5N118, SN74CB3Q3251, SN74CBT3251

hi,

advance thanks for reply, i need the analog multiplxer for 16:1, it can support switching current for above 60mA, so please suggest the part number for my requirement.

regards,

sankar

  • Hello Sankar,

    Unfortunately we only have single channel 8:1 switches which can support 60mA or more of continuous switching current. You did not indicate a voltage range you would be operating in so I have taken the liberty of attached snippets from 3 datasheets with 8:1 multiplexers supporting 60mA and up.

    The first part is the TS5N118 which has a recommended Vcc of 4.75V to 5.25V, with absolute maximum rating for switch current of 100mA:

    The next part is the SN74CB3Q3251, with a recommended Vcc of 2.3V to 3.6V, ON-state switch current of 64mA (MAX):

    and third, the SN74CBT3251, with a Vcc of 4V to 5.5V, with MAX continuous channel current of 128mA:

    Thank you, 

    Louie

    If I have answered you question, please hit the Verify Answer button

  • Please see instructions below for looking up parts within our portfolio:

    Go to this URL:

    Once you are there on the right side, you can select configurations you care about, number of channels (Highlighted section)

    then click the red view button which will be in any of the filter sections (circled in blue):

    This will speed up any searches you have in our portfolio, so you are not delayed waiting for a response from our team.

    Thank you,

    Louie