Other Parts Discussed in Thread: SN74CB3Q3257,
The questions is a recommended treatment of unused xA and xBx pins of SN74CBT3257. Since SN74CBT3257 is an analog switch and those pins are bidirectional actually, I’d like to confirm if there is a recommended way to prevent latch up or problematic behavior according to its internal circuit.
The customer uses only the channel #1 and #2. The pins 3A and 4A are treated as open left unconnected and pins 3Bx and 4Bx are pulled down to ground through 10k ohm resistor Could you please let us know your recommendation?
Thank you,
Adam