Hello,
Regarding to SN74LV4051, my customer is asking a question.
(Question)
When minus signal(0> Vio> -0.5V) is input, is output minus signal?
(For example: -0.2V -> Y0 pin-> COM pin -> -0.2V? )
On their application, it is possible that minus signal is input.
If this device is supported bidirectional, I guess that output will be minus signal at inputting minus signal.
Of course, we should consider Absolute Maximum Ratings (Vio> -0.5V).
Is this device is supported bidirectional?
And My understanding is correct?
Regards,
Tao2199