Other Parts Discussed in Thread: CD4053B, CD4052B,
Hi all
Would you mind if we ask CD4051B, CD4052B and CD4053B?
<Question1>
RDS is 470ohm(typ) upto 1050ohm(max) in case of 25C.
So, if the device'S RDS is 1050ohm@25C, in case of 125C, RDS will be 2.5kohm?
Or, including above mention, in case of 125C, MAX RDS is 1.3kohm?
<Question2>
If this device has diode clump inside, do you have follows charactics?
-VF-IF charactics
-IR-VR charactics
<Question3>
About output capacitance, do you have Electrical Characteristics in case of 125C?
Kind regards
Hirotaka Matsumoto