Part Number: SN74CBTLV3251
Hallo
I am performing the testing of multiplexer via microcontroller. I am providing the logic for address/select lines via Microcontroller GPIOs. But while testing I am facing the problem that my multiplexer is only giving output to 8(B8) pin as it is 1:8 MUX. In spite, I am changing the logic of address lines via microcontroller, the Multiplexer is only connecting its input to 8th output pin. The multiplexer I am using is from Texas Ins. SN74CBTLV3251.
Can somebody suggest what could be problem ??
Thanks in advance