Other Parts Discussed in Thread: TINA-TI, TS5A23166
I designed a 3306 into a analog bus isolation application. Device is powered with 5V and I'm trying to pass 0-5V signals through it. I've noticed when the signal I'm passing is between 3.75-5V, the device clamps the output to 3.75V.
My initial though is that this is some type of diode clamp or maybe the -2v overshoot protection kicking in, but in any case its very frustrating. This product was found in the analog switch/multiplexer family on ti.com and the datasheet and product page specify 5V output levels. I also didn't see a spice model on the product page, but I'm downloading Tina-TI just incase its included with the package.
Could someone clarify why this is happening?
Thanks,
Trey