Hi,
I'd like to test several resistive sensors versus temperature. Outside of the climatic chamber I'll have a board (Arduino driven) that will switch the precision ampermeter to each sensor.
The only issue I see is the leakage current of the chosen multiplexer: SN74CBT3251. The only figure related I found in datasheet is Ii=+/-1µA max. I'm not sure of what it means.
In my setup I'll have:
- on common pin: a voltage generator of 1V
- on each output of the multiplexer: a sensor of about 1Mohm.
Actually, the setup is differential, so it's the same on the other side of the sensor exept the common pin is connected to the return of the voltage generator.
What should I expect as measurement error in this setup? If there is 1µA on each "off" output and 1µA (1V/1Mohm) on my "on" input it does'nt sounds good :/
But there is still a chance to keep this setup as my only concern is relative measurement so if the leakage is independant of the output load it should be ok. Is it?
Last question: How variable is the leakage current from one output to the other? Maybe I can, measure with a precision 1Mohm and then juste calibrate the error?
Any suggestion is welcome,
Thanks for your help,
Thomas