Other Parts Discussed in Thread: SN74CBT3305C, SN74CB3Q3305
Hello guys,
The following is a question about SN74LVC2G66 from one of our customers. Could you please give me your answer for the customer?
Ques: We can see the sentence "Inputs and outputs are overvoltage tolerant allowing them to go as high as 5.5 V at any valid VCC." on page14 in the device datasheet (SCES325L). Is this correct. I think it is correct for control input terminals (1C,2C). But I think it should be not correct for I/O terminals (1A,1B,2A,2B) because the absolute maximum rating table says Switch I/O voltage= –0.5 ~ VCC + 0.5 V. Is my understanding correct?
Your answer would be much appreciated.
Best regards,
Kazuya Nakai.