This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bus Switch solution for Quad SPI

Guru 19655 points
Other Parts Discussed in Thread: TS3A27518E, SN74CBT16214, TS3USB3031

If there recommended bus switch for Quad SPI, please let me know.

(I didn't find match device)

Customer condition is below;

-----------------------------------

・Master: 1, Slave: 3

・Master's I/O port is connecting these Slave side and ON/OFF switch by bus switch.

・Always communicate one-Master and any one-Slave, the other Slave are switch OFF.

-----------------------------------

Best regards,

Satoshi

  • Satoshi-san,

    Why can't you have the master and the 3 slaves all on the same bus and use the chip select bit (/CS) defined in the qSPI protocol to determine which slave to select?  Are you I/O limited to communicate to the slave devices?  

    When I searched the switches and multiplexers forum for qSPI, I found several posts around the TS3A27518E device.  This is a 6-channel device which switch means it can switch all six bits of the SPI protocol 4 data lanes, clock, and /CS.  

    The TI switch portfolio offers 7 different 3:1 devices.  To cover all 6 bits of qSPI you will need to use 3x TS3USB3031 devices or 1x SN74CBT16214 with 6 unused channels. 

    Let me know if these will work in your system.

    Thank you,

    Adam