This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A5223: Replace TS3A5223 with lower cost version of 2-channel 2:1 multiplexer to mux inputs from BT chip

Part Number: TS3A5223
Other Parts Discussed in Thread: TS5A23157

e2e,

Please recommend a device that will replace the TS3A5223 with a lower cost version.  I need a low cost DPDT analog switch to mux the analog inputs of BT chip.  I need it to operate at 1.8V logic level.  I do not need it to be high speed or super low resistance.

Thank you,

Adam

  • Hello Adam,

    Thank you for the request. ti.com has since updated its product page and searching for such a part is very easy.

    Please see the snippet below where I filtered the offered portfolio by the configuration you requested to best match the TS3A5223 functionality.

    I then sorted the list based on the the price since you are looking for more a device which is cost efficient.

    I circled the parameters which I searched and then highlighted any specs which might be of interest to you.

    I would suggest the TS5A23157, our lowest costing device which will operate with 1.8V logic.

    Thank you,

    Louie