Hi..
i am using SN74LVC827APWR with 10input & 10 output buffer, to drive reset signals to 10# high speed signal cards by using signal reset switch .
Requirement :
Reset signal voltage level is 1.8v (VCC)
Reset switch ouput is shorted to all 10 input of this buffer.
i planned to short all outputs of the buffer so that i can achieve the highest drive current at the output as well as required current to drive 10# different high speed signal cards.
if it is not possible in the above part (SN74LVC827APWR) please suggest me any other part where i can able to short all the inputs to single reset in signal and all the outputs to single reset out in order to achieve the required drive strength.
Thanks & regards,
Divya