The customer is asking whether IN port of TS12A12511 can support 3.3V or not? According to the datasheet, it seems the IN port support only 5V, but could you tell me whether 3.3V is available on IN port, or not?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The customer is asking whether IN port of TS12A12511 can support 3.3V or not? According to the datasheet, it seems the IN port support only 5V, but could you tell me whether 3.3V is available on IN port, or not?
Shashank,
The switch's logic control pin IN is referenced to GND and the Vih value will scale with Vcc. You can see in the datasheet that with Vcc = 5 V and -Vcc = -5V the Vih spec is 2.4 V and will support your 3.3V logic control signal.
If the Vcc = 12 V than the Vih spec is 5V which will not support 3.3 V control logic signals.
I searched "TS12A12511" in the switches and multiplexers e2e forum and found these post that may also be helpful.
Thank you,
Adam