Hi Team,
Do we have below switches?
1. One is 4 to 8 differential pair switch, support USB3.1 and DP1.2
2. The other one is 4 to 2 differential pair switch, support USB3.1.
Thanks very much!
Nic
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Do we have below switches?
1. One is 4 to 8 differential pair switch, support USB3.1 and DP1.2
2. The other one is 4 to 2 differential pair switch, support USB3.1.
Thanks very much!
Nic
Hi Nic,
1) My assumption is that you're looking for Type-C ALT mode devices, in which case please take a look at HD3SS460 which is for either source or sink applications, TUSB546A-DCI and TUSB1046A-DCI which are for source applications and TUSB564 & TUSB1064 for sink applications.
2) For Type-C we have many options such as HD3SS3220 which has DRP port controller integrated, HD3SS3212, TUSB1042I with linear redriver & TUSB542 with linear redriver also.
Regards.
JC