Hello,
Can you please help provide the T&R spec for the TS3DDR4000?
Thanks,
Celi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can you please help provide the T&R spec for the TS3DDR4000?
Thanks,
Celi
Celi,
Thank you for bringing this to our attention that the tape and reel dimensions are missing from the datasheet. I will work on getting these back into the datasheet.
Ao= 3.40mm +/-0.1
Bo= 8.40mm +/-0.1
Ko= 1.65mm +/-0.085
The pocket dimensions above refer to the widest part of the pocket. The pocket is designed so that the IC will sit on the angled bevel.
Thank you,
Adam