Other Parts Discussed in Thread: CD4502B, MUX507
Hello,
I am considering the CD4052B (multiple in parallel) to use in switching 60 transducers between different connections. This purpose would require the disabled chips to be very high impedance.
My issue right now is the data sheet says that the chip has a very high OFF state resistance. With the chip we currently have and are testing right now, when the chip is inhibited, it is still drawing a considerably large current (more than the pA range suggested in the data sheet).
I would like to know what the chip/circuit looks like inside when it is disabled, and where the input goes in this mode? And if I could get the specific value of the input resistance in the OFF mode. I am currently using 1.5MHz signals with the device.
Thanks