Other Parts Discussed in Thread: TS3L301, , TS3DV642
Hi,
Do you have a switch/MUX that supports SGMII?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Do you have a switch/MUX that supports SGMII?
Thank you
Whitney,
To determine if a signal switch can support a signal standard you need to evaluate the number of bits/channels needed to switch, the voltage level, and the bandwidth.
SGMII looks to be a 12 bit/channel signal path, voltage levels of 2.5V or 1.5V, and speeds of up to 125MHz.
The TS3L301 meets the voltage and bandwidth requirement but is only 8-channel/bits. 12 channel devices would include devices like TS3DV642 or TS3DDR4000. Let us know what you think.
Thank you,
Adam