This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We need a MUX to fulfill UART 1:12 MUX function. Do you think we can use two CD74HC4067 chips (one for UART TX and one for UART RX) to make it? Please let me know if there's a better option.
Thanks!
Antony
Antony,
If you're UART signal voltage and bandwidth is within the recommended operating conditions and your system can handle ~60 ohm series resistance the CD74HC4067 can work.
Most switches can support UART signals because of their low speeds and we even new ones like the TMUX136 (2-channel, 2:1 mux). Unfortunately, our portfolio doesn't have many options for 12:1 mux.
What you're you trying to communicate with that uses so many UART signals?
Thank you,
Adam