This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to use the TS5A3359 SP3T switch in an analog circuit. I see that the analog signal range of the switch is 0 to VDD. My signals are sinusoids oscillating about GND, so in the range of +-2V incming on the NO0, NO1 and NO2 ports.
So as to not have the negative part of the signal attenuated, I was wondering if I could give the switch a +-2.5V dual supply instead of a 0 to 5V supply. Would that make my signal with a negative oscillation component ok for use with this switch?
Thanks
Kanika
Kanika,
Yes, it is possible that you can bias the switch with +/-2.5V instead of 5V but you must be cautious that all the datasheet values are now referenced to -2.5V instead of 0V. You will need to keep this new reference in mind for things like Vih and Vil which will now be shifted by -2.5 V.
Thank you,
Adam