Hi
What's the output impendence of SN74LVC1G66 in OFF state? Is it high impendence or some certain high low state? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
What's the output impendence of SN74LVC1G66 in OFF state? Is it high impendence or some certain high low state? Thanks.
Wayne,
The SN74LVC1G66 is a passive FET switch with the I/Os being the drain and source of the FET. When the switch is in the off state the channel of the FET connecting the drain and source is removed and places the impedance between the I/Os Hi-Z. This device does not have any drive capability.
You can find more information in the switches and mutliplexers FAQ.

Why did you pick the SN74LVC1G66 for your application? What are you connecting to the I/Os of the device?
Thank you,
Adam
Adam
Thanks for your so detailed answers.
This part is to be used as a 1V analog signal switch, the receiver is GPIO of MCU.