Part Number: TS5A9411
Other Parts Discussed in Thread: TS12A12511, TLV171
Hi,
I have a couple of voltage and current interfacing questions regarding the TS5A9411:
1) Is this switch suitable for switching a signal to a micro ADC?
2) With VCC (+5V) and GND (0V) can I supply COM, NO and NC DC voltages from -5V to +5V?
3) Can I drive the IN pin with the output of an LM393AD comparator. The datasheet quotes the LM393AD can drive a max of 20mA.
3) Am I understanding the datasheet correctly and thinking NC, NO and COM can supply a maximum of 200mA?
Thanks,
Rocketman46