Part Number: CD4097B
Other Parts Discussed in Thread: MUX507
Dear Sir, please answer
I'd like to use CD4097B as (8:1)x2 analog multiplexer.
I have dual +/- 5 V power supply (+5V, -5V, GND).
I need to tranfer 15 mV.....3V, 50 Hz differential signal through CD4097B. I take this differential signal from current trasformer. I need to feed this signal (after CD4097B) to differential amplifier with +5V, -5V supply.
1) If I understand right, for feeding "0" logical level to A, B, C,INH inputs, then I need to feed minus 5V voltage to A, B, C,INH. For feeding "1" logical level to A, B, C,INH inputs, then I need to feed 5V voltage to A, B, C,INH. Am I right?
2) But maybe I can feed 15 mV.....3V, 50 Hz differential signal to CD4097B using single supply 10V ( Vss=0V, Vdd=10V)? But I suppose that it is impossible.
3) Please, recommend any IC for controlling A, B, C, INH inputs.
TIA
Sincerely,
Vladimir Naumenkov
www.agat.by